earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation, WebStation
Functionalities: Basic Functionality, Graphics
12/11/2025

Fire Graphic Menus

arrow1_rotationShow Menu arrow1_rotationStatus Menu arrow1_rotationActions Menu

The graphic menus in EcoStruxure Fire Operation are used to display alarms and alerts in a graphic. The menus are also used to execute commands on loop devices and zones, or on the fire detection system.

Show Menu

In WorkStation or WebStation, in a fire graphic, you use the Show menu to display, hide, or search for addresses and zones.

 
action_zoom_plus_stroke Show menu
Figure: Show menu

For more information, see Displaying and Searching for Loop Devices and Zones in a Graphic .

Status Menu

In WorkStation or WebStation, in a fire graphic, the Status menu displays the number of active alarms and alerts on loop devices and in zones. The category of alarms and alerts has a certain color, which is displayed on the loop devices and zones having alarms or alerts in that category.

 
action_zoom_plus_stroke Status menu
Figure: Status menu

Actions Menu

In WorkStation or WebStation, in a fire graphic, you use the Actions menu to disable and enable loop devices and zones in the graphic. On loop devices, you turn external output relays on and off. You also request address updates on loop devices. By executing system commands, you affect different categories of alarms and alerts in the entire fire detection system.

 
action_zoom_plus_stroke Actions menu
Figure: Actions menu

For more information, see Saving a Selection of Loop Devices In a Graphic .

For more information, see Deleting a Selection of Loop Devices in a Graphic .

For more information, see Turning External Output Relays On or Off from a Graphic .

For more information, see Disabling a Loop Device or a Zone from a Graphic .

For more information, see Enabling a Loop Device or a Zone from a Graphic .

For more information, see Requesting an Address Update on Loop Devices from a Graphic .

For more information, see Executing System Commands from a Fire Graphic .

  • How Graphics Work in Fire Operation