earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation, WebStation
Functionalities: Basic Functionality, Graphics
10/10/2025

Enabling a Loop Device or a Zone in a Graphic

You enable a loop device or a zone to make them operate in the fire detection system.

Warning Warning

COMPROMISED FUNCTIONALITY

Ensure that no obstructions preventing normal operation are present before you enable loop devices or zones.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Important:

Ensure that there is no smoke, dust, or any other condition, near the loop device or in the zone, that can affect the fire detection and result in a false alarm.

To enable a loop device or a zone in a graphic
  1. In WorkStation or WebStation, in a fire graphic, click a disabled loop device or zone.

  2. On the Actions menu, click the Enable/Disable button, which displays the current state (disabled) of the loop device/zone:

     
    action_zoom_plus_stroke

  3. Click the Apply button

     
    action_zoom_plus_stroke
    to enable the loop object.

If there are no remaining disablements on the object, it is enabled and the updated state is visible in the graphic.

  • Fire Graphic Menus