Executing System Commands from a Fire Graphic
You execute system commands to reset, silence, or re-sound alarms or alerts in the fire detection system.
Warning
|
REDUCED RESPONSE TO FIRE
Ensure that there is no need for evacuation before you reset or silence alarms or pre-alarms.
Comply with any applicable legislation, regulations, standards and/or guidelines regarding actions to be taken before you reset or silence alarms or pre-alarms.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
|
Important:
Executing a system command affects the entire fire detection system, not only what is displayed in the graphic.
To execute system commands from a fire graphic
In WorkStation or WebStation, in a fire graphic, in the
Actions
menu, click the system command button
action_zoom_plus_stroke
.
To execute reset commands, click the
Reset
button
action_zoom_plus_stroke
and then select the command you want to execute.
To execute silence commands, click the
Silence
button
action_zoom_plus_stroke
and then select the command you want to execute.
To execute re-sound commands, click the
Re-sound
button
action_zoom_plus_stroke
and then select the command you want to execute.
Click the
Apply
button
action_zoom_plus_stroke
to execute the command.
Fire Graphic Menus