earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, Enterprise Central, Enterprise Server, FDP Server, Function Block Editor, Graphics Editor, ​License Administrator, ​License Server, Script Editor, Software Administrator
Functionalities: Basic Functionality, License Management, Localization
12/5/2025

Installation and Upgrade Overview

arrow1_rotationInstallation Overview arrow1_rotationUpgrade Overview arrow1_rotationLicensing Overview

To run the EcoStruxure Building Operation software, you need to install and license the software. To keep your system maintained and up to date, you need to upgrade the software.

Installation Overview

The EcoStruxure Building Operation software products are installed using installation packages.

For more information, see Installation Overview .

Upgrade Overview

A system upgrade can include an Enterprise Server, one or more field servers and WorkStations, and the supporting administrator software, such as Device Administrator.

Licensing Overview

The EcoStruxure Building Operation software is available for all to download and install. However, you need valid licenses to use the software. The number of users of the software is limited to the number of licenses owned by the customer.

For more information, see Licensing Overview .

  • EcoStruxure Building Management Overview
  • Installation Overview
  • Licensing Overview