earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Graphics
10/30/2025

Resetting Zoom in a Graphic in WebStation

You restore the graphic to its original size after you increased or decreased the size of the graphic.

Show More
action_close

You use graphics to display building overviews, display the status of detectors and alarms, display the value of sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.

A graphic that contain links to documents, such as Microsoft Word or Adobe PDF, can be opened in WorkStation and WebStation. The associated programs, in this case Microsoft Word or Adobe Reader, has to be installed on the computer running WorkStation or WebStation.

 
action_zoom_plus_stroke A Graphic with links and interactive components like gauges in WorkStation
Figure: A Graphic with links and interactive components like gauges in WorkStation

Show More
action_close

You use graphics to display building overviews, display the status of detectors and alarms, display the value of sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.

A graphic that contain links to documents, such as Microsoft Word or Adobe PDF, can be opened in WorkStation and WebStation. The associated programs, in this case Microsoft Word or Adobe Reader, has to be installed on the computer running WorkStation or WebStation.

 
action_zoom_plus_stroke A Graphic with links and interactive components like gauges in WorkStation
Figure: A Graphic with links and interactive components like gauges in WorkStation

Fire Graphic Headers

If a default graphic is defined in the fire detection system configuration, the Home button

 
action_zoom_plus_stroke
in the fire graphic header displays the default graphic.

If a navigation menu is created in the fire detection system configuration, the Navigation button

 
action_zoom_plus_stroke
in the fire graphic header displays the navigation menu.

Fire Graphic Menus

The graphic menus in EcoStruxure Fire Operation are used to display alarms and alerts in a graphic. The menus are also used to execute commands on loop devices and zones, or on the fire detection system.

For more information, see Fire Graphic Menus .

Sets of Icons in Fire Graphics

There are three sets of icons in fire graphics: default icons, Swedish icons, and Finnish icons. In Fire Expert Graphics manager, you choose which icon set you want the graphics to use.

For more information, see Sets of Icons in Fire Graphics .

To reset zoom in a graphic in WebStation
  • Right-click in the graphic and click Reset zoom .

  • How Graphics Work in Building Operation
  • How Graphics Work in Fire Operation
  • Edit Properties Dialog Box
  • Changing a Value in a Graphic
  • Zooming and Scrolling in a Graphic in WebStation