Use this workflow to assign and activate licenses on field servers that are not connected to Internet and cannot access License Activation Server (FNO).
Do not use this workflow if you are on a semi online system where the field servers are not connected to Internet, but the Device Administrator is connected to the Internet.
For more information, see Semi Online System .
You need one computer running Device Administrator that is connected to Internet.
Related information can be found in the sections after the flowchart.
Install certificates if you use HTTPS for communication.
For more information, see Device Administrator Certificate Workflow .
Make sure that you have the Entitlements containing the licenses. You need the email with the entitlement during the process.
For more information, see Order Information Request .
In Device Administrator, you add entitlements that contains products and licenses.
This is done so that you can view all licenses that are available to be assigned and then activated.
Make sure that you have the HTML entitlement certificate file or the entitlement ID available .
There are two different procedures to add and set up an entitlement:
When the HTML entitlement certificate file is available.
For more information, see Adding an Entitlement using the HTML file when a Field Server is not Connected to License Server (FNO) .
When the HTML entitlement certificate file is not available you must use the entitlement ID.
For more information, see Adding an Entitlement without the HTML file when a Field Server is not Connected to License Server (FNO) .
Use the License Products available in the entitlements to assign License Features to the field servers.
For more information, see Assigning Licenses .
Create request files with the licenses you want to activate.
You gather, and download, the license information from the field servers. This information is used to identify the licenses that is to be reclaimed from the License Activation Server.
For more information, see Creating the Request Files .
Activate the request files on License Activation Server (FNO) to receive response files.
This step must be done a computer that is connected to Internet and has access to License Activation Server.
Send the response files to the field servers to complete the activation.
You gather, and download, the license information from the field servers. This information is used to identify the licenses that is to be reclaimed from the License Activation Server.
For more information, see Sending the Response Files to the Field Server when Activating or Reclaiming Licenses .
After the licenses has been installed, make a backup of the field server to make sure that you do not lose the licenses if any problems occur.
For more information, see Backup .