earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Device Administrator, FDP Server, ​License Administrator
Functionalities: Engineering
3/6/2025

Creating the Request Files when Reclaiming Licenses

You create request files to get a response file with reclaimed licenses from License Activation Server (FNO).

You gather, and download, the license information from the field servers. This information is used to identify the licenses that is to be reclaimed from the License Activation Server.

Show More
action_close

You can reclaim licenses on your field servers so that the licenses are updated with the latest information.

This is typically done when expanding a license subscription.

Reclaim licenses on field servers

Device Administrator is used to reclaim licenses installed field servers.

Consider the following cases when reclaiming licenses on field servers.

Online

In the online case the computer that runs Device Administrator is connected to the Internet.

For more information, see Reclaiming Licenses for Licenses on Field Servers Connected to Internet .

Online reclaim on a semi online system

A special case is semi online system where the field server is not connected to Internet, but Devices Administrator is connected to Internet. A semi online system is treated as an online system for licensing purposes.

For more information, see Semi Online System .

For more information, see Reclaiming Licenses for Licenses on Field Servers Connected to Internet .

Offline

In the offline case the computer that runs Device Administrator and the field servers are not connected to the Internet. Neither the Device Administrator nor the field servers can connect to License Activation Sever (FNO).

Use this workflow to reclaim licenses on field servers that are not connected to Internet and cannot access License Activation Server (FNO).

For more information, see Reclaim Licenses for Licenses on Field Servers not Connected to Internet (FNO) Workflow .

Reclaim licenses on Enterprise Central or Enterprise Servers

License administrator is used to reclaim licenses installed on Enterprise Central or Enterprise Server.

For more information, see Reclaiming Licenses for Licenses on License Administrator .

To create the request files
  1. In Device Administrator, click Servers .

  2. Select Show Licenses .

  3. Select the field servers.

  4. Click Reclaim .

  5. Click Create request files .

  6. Click OK .

  7. In the License Information field, browse to the license information file.

  8. In the Request field, browse to the location where you want to download the request file information file

  9. Click Download .

Move the request file to a computer running Device Administrator that is connected to Internet.

  • Field Server Licensing Overview
  • Reclaim Licenses
  • Reclaim Licenses for Licenses on Field Servers not Connected to Internet (FNO) Workflow
  • Gathering Server Information
  • Creating the Request Files when Reclaiming Licenses
  • Downloading License Information
  • Uploading Request Files to License Activation Server (FNO)
  • Sending the Response Files to the Field Server when Activating or Reclaiming Licenses