earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Security
10/30/2025

Security Banner 

A security banner is displayed when a user enters a secure system. The security banner notifies the user of the legal rights connected to the use of the information in the secure system.

The banner is displayed for all users that enter the system regardless of their domains or rights and regardless of if they enter using WorkStation or WebStation.

Important:

WebStation users are logged off from WebStation when they reload a page if they are a member of a group where the group members are automatically logged off and the security banner is displayed.

  • Security Overview
  • Adding a Security Banner 
  • Removing a Security Banner