earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Security
5/7/2026

Security Overview

arrow1_rotation Firewall arrow1_rotation Password Policy arrow1_rotation Embedded Content in WebStation arrow1_rotation Automatic Log Off arrow1_rotation Security Banner arrow1_rotation Certificates arrow1_rotation Certificates and SSL Security in Device Administrator arrow1_rotation Encrypted Communication arrow1_rotation Web Server Access Logging arrow1_rotation Field Server Remote System Logging arrow1_rotation Connect Agent arrow1_rotation Document Policy arrow1_rotation Disable Field Server Ports arrow1_rotation Change Control arrow1_rotation Multi-factor Authentication

EcoStruxure Building Operation software has a number of features that helps you increase the security in your system.

Firewall

You can configure the devices that are allowed to communicate with the field server to prevent connection attempts from unauthorized devices. The IP addresses of the devices that are allowed to communicate with the field server are added to the whitelist.

Password Policy

You can increase the password security by configuring a password policy that defines how passwords must be created by the users.

For more information, see Password Policy .

Embedded Content in WebStation

For security reasons, the default setting is for WebStation to not be embedded in another web site and for other contents to not be embedded in WebStation. However, you can change this security setting in WorkStation.

For more information, see Security Configuration in WebStation .

Automatic Log Off

The automatic logoff function makes it possible for the system to automatically log off a user after a specified time of inactivity.

Security Banner

A security banner is displayed when a user enters a secure system. The security banner notifies the user of the legal rights connected to the use of the information in the secure system.

For more information, see Security BannerĀ  .

Certificates

The EcoStruxure Building Operation software supports certificates. Certificates are electronic credentials that are used to certify the identities of computers, and other entities on a network.

For more information, see Certificates .

Certificates and SSL Security in Device Administrator

You can increase the security between the Device Administrator and field servers using certificates and SSL security configuration.

For more information, see Certificates and SSL Security .

Encrypted Communication

To increase the security of your data, you can disable incoming HTTP communication and allow only high security communication.

For more information, see Disable HTTP Communication .

Web Server Access Logging

You can log all web server HTTP access to the Enterprise Server and the Enterprise Central.

For more information, see Web Server Access Logging .

Field Server Remote System Logging

You can log all successful and unsuccessful attempt to log on to your field server.

Connect Agent

To prevent data transfer over the cloud server, you can disable the transfer of system information and crash information of the Enterprise Central and the Enterprise Server and its field server.

Document Policy

You can increase the security in your system by configuring the document policy. The document policy controls which file types a user can open, save, and import.

For more information, see Document Policy .

Disable Field Server Ports

You can disable port 22 and the USB ports on the automation server.

Change Control

Change Control is a way to require that a user add a comment and signature for changes made in the system.

For more information, see Change Control .

Multi-factor Authentication

You can use multi-factor authentication to increase the security in your system.

For more information, see Multi-factor Authentication .

  • Password Policy
  • Security Configuration in WebStation
  • Security BannerĀ 
  • Certificates
  • Disable HTTP Communication
  • Web Server Access Logging
  • Document Policy
  • Change Control
  • Multi-factor Authentication