earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Security
10/30/2025

Disabling MD5 Hash

You disable MD5 hash when you want the EcoStruxure BMS servers to use only strong algorithms for encryption.

Show More
action_close

To increase the security of your data, you can disable incoming HTTP communication and MD5 encryption.

Disable Incoming HTTP Communication

You disable incoming HTTP communication to increase the security of your system. Only the incoming communication is affected, so EcoStruxure Building Operation software still works as an EcoStruxure web service client.

When HTTP is disabled, HTTPS must be used between EcoStruxure BMS servers and clients like WebStation and WorkStation. Between EcoStruxure BMS servers, HTTPS or TCP must be used. Ensure that the communication protocol HTTPS between servers is secure.

An EcoStruxure web service client using HTTP cannot receive information from an EcoStruxure BMS server on which incoming HTTP communication is disabled. An EcoStruxure web service client using HTTPS can still receive information from an EcoStruxure BMS server on which incoming HTTP communication is disabled.

For more information, see Disabling Incoming HTTP Communication .

Disable MD5 Hash

If you want the EcoStruxure BMS servers to use only strong algorithms for encryption, such as AES128 and SHA256, you have to disable MD5 hash. MD5 hash must be disabled for you to use Federal Information Processing Standards (FIPS).

For more information, see Disabling MD5 Hash .

Redirect Web Client to HTTPS

You can force users to only use HTTPS when they access an EcoStruxure BMS server using WebStation.

For more information, see Redirecting Web Clients to HTTPS .

To disable MD5 hash
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Security Settings .

  4. In the Security Manager , clear Allow authentication with MD5 hash .

  5. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Encrypted Communication
  • Security Settings – Control Panel