Log on to rate and give feedback
12345Log on to rate
0
How to
Products:
WebStation
Functionalities:
Trends
12/2/2024
Showing Tooltip for the Closest Item
Use the Magnetic function to view the value closest to the pointer.
Show More
action_close
You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.
These settings can be saved so that the trend chart is displayed in the same way anytime you open it.
To show tooltip for the closest item
In WebStation, in the
System tree
pane, select the trend chart.
Click the
Show tooltip for the closest item
button