earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server, ​License Administrator, ​License Server
Functionalities: License Management
2/27/2025

License Information

arrow1_rotationLicense Information on Servers arrow1_rotationLicense Status

The License Information in the Control Panel gives you an overview of the licenses in your EcoStruxure BMS.

License Information on Servers

License Information is found in the Control Panel for every EcoStruxure BMS server but the information is slightly different for every server.

Enterprise Central

Enterprise Central displays all licenses for Enterprise Central. The License Information in Enterprise Central also displays information regarding all Enterprise Servers attached to the Enterprise Central and for all field servers attached to the Enterprise Servers.

In the License Information in Enterprise Central, you can select a specific Enterprise Server and check the licenses for that server.

For more information, see Licenses Administrated by License Administrator Overview .

Enterprise Server

Enterprise Server displays all licenses for the Enterprise Server and the attached field servers.

For more information, see Licenses Administrated by License Administrator Overview .

Field server

Field server displays all licenses for products in used in the field server.

For more information, see Centralized Licensing Overview .

License Status

Licenses can have the following status:

  • Required : Displays the number of licenses that are required for your EcoStruxure BMS.

  • Used : Displays the number of licenses that are currently in use for your EcoStruxure BMS. If this number is lower than the number in Required, a license violation is displayed in the License Information. A License Violation bar is also displayed in WorkStation. For more information, see License Violation Bar .

  • Available : Displays the number of available licenses that are activated on the License Server but not in use in your EcoStruxure BMS.

  • Activated : Displays the total number of licenses that are activated on the License server, used and unused.

  • License Information Enterprise Server
  • License Information Enterprise Central
  • Licensing Overview