earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Trends
12/3/2024

Configuring a Trend Log Series in a Multi Trend Log List 

You configure an individual trend log series in a multi trend log list to change how the values of the trend log series are presented in the multi trend log list.

Important:

When you edit an individual trend log series, the changes are overridden by any configuration on the multi trend log list.

Show More
action_close

You configure a multi trend log list to display values from multiple trend logs in one list. You compare values in a multi trend log list when you commission or validate an EcoStruxure BMS.

For example, on a b3 BACnet device, there are two inputs: SpaceTemp and SpaceHumidity. Both inputs have logs set up intrinsically. You want to print the last 3 days of history for these inputs. You create a multi trend log list for both inputs. You can export the multi trend log list to a .CSV file or an .XML file, or .XLSX file, and then use an external editor to compare the values.

If a trend log has no available value for a given time stamp in a multi trend log list, then the trend log displays an empty cell for that specific time. You can fill that empty cell with the latest known value.

You can change the column order in the multi trend log list and save the change.

You can add, edit, or remove trend logs from the multi trend log list at any time. You can also edit how trend logs are displayed in the multi trend log list. For more information, see Configuring a Trend Log Series in a Multi Trend Log List  .

Tip:

You can add a trend log to a multi trend log list using drag and drop.

You can configure the individual trend log series in a multi trend log list.

Important:

All configurations on individual trend log series are overriden if you configure the multi trend log list.

Temporary multi trend log list

You can view a group of trend log lists in a atemporary multi trend log list without creating a multi trend log list. For more information, see Viewing Trend Logs in a Temporary Multi Trend Log List  .

Time Zone Modes in a Trend Log List

​In a trend log list, you can present the records of a trend log in different time zones: local time zone, EcoStruxure BMS server time zone, and UTC time zone.

For more information, see Time Zone Modes in a Trend Log List .

Calculation Methods

​Use a calculation method to process the records of the trend log before presenting them in a trend log list or a trend chart. The original records in the trend log are not affected by the calculation method. The calculation method is applied to the trend log records grouped by a specific time interval.

For more information, see Calculation Methods .

Important:

If you have selected a calculation method on a series, event icons are not displayed on that series in the multi trend log list.

Floating Point Values NaN, INF, and -INF

In the EcoStruxure BMS software, the floating point values “Not a Number”, positive infinity, or negative infinity may be displayed in the Basic property tab, in a trend log list, or a trend chart.

For more information, see Floating Point Values NaN, INF, and –INF .

To configure a trend log series in a multi trend log list 
  1. In WorkStation, in the System Tree pane, select the multi trend log list containing the individual trend log series whose properties you want to edit.

  2. In the Multi trend log list viewer, on the toolbar, click the Open multi trend log list settings button

     
    action_zoom_plus_stroke
    .

  3. In the Multi Trend Log List Settings dialog box, click the Series tab.

  4. Edit the series properties:

    Table: Multi Trend Log List Settings – Series Tab

    Property

    Description

    Data series

    Select the individual trend log series whose properties you want to edit.

    Display trend log

    Displays the selected trend log in the Data series list.

    Calculation method

    Select a calculation method.

    For more information, see Calculation Methods .

    Delta over period

    Select True to apply a period to the delta calculation method.

    For more information, see Calculation Methods .

    Period

    Select the time span for which the calculation method is to be executed.

    Custom period

    Enter a custom time span for which the calculation method is to be executed.

    Custom period alignment

    Enter the time when you want the custom period to start.

  5. Click OK .

  • Multi Trend Log Lists
  • Calculation Methods
  • Adding a Trend Log to a Multi Trend Log List 
  • Removing a Trend Log from a Multi Trend Log List 
  • Configuring a Multi Trend Log List 
  • Multi Trend Log Settings Dialog Box – Series Tab
  • Multi Trend Log List Series Properties
  • Multi Trend Log Settings Dialog Box – General Tab