earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
12/3/2024

Configuring an Alarm Triggered Notification 

You configure an alarm triggered notification to notify users when an alarm condition is met.

To configure an alarm triggered notification 
  1. In WorkStation, in the System Tree pane, select the alarm triggered notification you want to configure.

  2. Click the Alarm Triggered Notification tab.

  3. Edit the properties:

    Table: Alarm Triggered Notification

    Property

    Description

    Status

    Select Disabled to deactivate the notification function.

    Activation schedule

    Enter the schedule that contains the value that activates the notification.

    Schedule value when active

    Enter the value, generated by the connected schedule or other multistate variable, that activates the notification.

    Report template

    Enter the path to the report template.

    For more information, see Notification Reports .

    Decimal symbol

    Select the decimal symbol to be used in the notification and the notification report template.

    Localization

    Select a language among the language packs installed on the EcoStruxure BMS server.

    System of measurment

    Select the system of measurements to be used in the notification report.

    Report format

    Select the format of the notification report.

    XLSX template

    Enter the path to the XSLX notification report template.

    Notification text

    Edit the notification text.

    Substitute missing data with

    Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all.

     
    action_zoom_plus_stroke

    Add

    Click to add a distribution method to the notification.

    For more information, see Notification Distribution Methods .

     
    action_zoom_plus_stroke

    Edit

    Click to configure the selected distribution method in the notification.

    For more information, see Notification Distribution Methods .

     
    action_zoom_plus_stroke

    Remove

    Click to remove the selected distribution method from the notification.

    For more information, see Notification Distribution Methods .

    Notify on transition to

    Select the alarm states that trigger the notification.

     
    action_zoom_plus_stroke

    Click to add an alarm filter condition for the notification. For more information, see Alarm Filters .

     
    action_zoom_plus_stroke

    Click to remove the selected alarm filter conditions for the notification.

     
    action_zoom_plus_stroke

    Clear all

    Click to remove all the alarm filter conditions for the notification.

  4. On the File menu, click Save .

  • Notification Reports
  • Document Signature Certificate
  • Create Object Wizard - Configure Write to File Page
  • Creating an Alarm Triggered Notification
  • Configuring a Variable Triggered Notification
  • Manually Triggering a Notification
  • Signing a PDF Notification Report with a Certificate