earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Alarms
12/3/2024

Document Signature Certificate

In EcoStruxure BMS, when you select the Write to File Notification Distribution Method and file format PDF, you can sign the notification report using a document signature certificate. . For more information, see Write to File Notification Distribution Method .

Document signing requires a certificate created with RSA.

You can choose to sign your notification report with a commercial CA certificate from MS Windows Certificate Store.

Document signature does not support Elliptic curve cryptography and therefore self signed certificates generated in the server cannot be used.

Important:

To use certificates from MS Windows Certificate Store, you need to ensure that the Windows Service User for the BMS EcoStruxure server has permissions to this store. Such a user account can be selected in Windows Services on your PC, or it can be done during installation and upgrade of the BMS EcoStruxure system. For more information, see Installing Enterprise Central .

  • Write to File Notification Distribution Method
  • Create Object Wizard - Configure Write to File Page
  • Certificates Tab
  • Signing a PDF Notification Report with a Certificate
  • Creating an Alarm Triggered Notification
  • Configuring an Alarm Triggered Notification 
  • Adding a Certificate using WorkStation
  • Generating a Certificate Using WorkStation