earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/2/2024

Getting Backup set from an EcoStruxure BMS Server using Device Administrator

You can create backup sets from an EcoStruxure BMS server using Device Administrator.

Show More
action_close

You can manually create backup sets using Device Administrator. The backup sets can be saved at any location. One or many EcoStruxure BMS Servers can be backed up at the same time.

To be able to create backup sets of an Enterprise Server or an Enterprise Central, you must run Device Administrator on the same computer as the Enterprise Server or Enterprise Central. You must also run Device Administrator as an administrator. Refer to Windows for information on how to run a program as administrator.

Note:
  • The attached automation servers of an Enterprise Server are not included in the backup set of an Enterprise Server.

  • The attached Enterprise Servers are not included in the backup set of an Enterprise Central.

For more information, see Getting Backup set from an EcoStruxure BMS Server using Device Administrator .

To get backup set from an EcoStruxure BMS server using Device Administrator
  1. In Device Administrator, click Servers and then select the EcoStruxure BMS Server(s).

  2. Click Get backup set .

  • Manual Backups
  • Local Backup of EcoStruxure BMS Servers using Device Administrator