earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server, WorkStation
Functionalities: Basic Functionality
12/3/2024

Display Names and IP Addresses of Servers Drop-Down List Box

You use the Display Names and IP Addresses of Server s drop-down list box to add, edit and delete the display names of the server addresses. You also use it to export, import and delete lists of the display names and IP addresses of servers.

 
action_zoom_plus_stroke Display Names and IP Addresses of Servers drop-down list box
Figure: Display Names and IP Addresses of Servers drop-down list box

Table: Display Names and IP Addresses of Servers Drop-Down List Box

Command

Description

 
action_zoom_plus_stroke

Edit

Click to edit the display name of the server address. For more information, see Editing the Display Name of the Server Address .

 
action_zoom_plus_stroke

Delete

Click to delete display name and the IP address of the server. For more information, see Deleting the Display Name and the IP Address of a Server .

 
action_zoom_plus_stroke

Export

Click to export the list of the display names and IP addresses of servers. For more information, see Exporting the List of the Display Names and IP Addresses of Servers .

 
action_zoom_plus_stroke

Import

Click to import a list of the display names and IP addresses of servers. For more information, see Importing a List of the Display Names and IP Addresses of Servers .

 
action_zoom_plus_stroke

Remove all

Click to the display names and IP addresses of servers. For more information, see Clearing the List of the Display Names and IP Addresses of Servers .

 
action_zoom_plus_stroke

Discover

Click to display servers from your network.

  • Log on to WorkStation or WebStation
  • Building Operation WorkStation Window
  • Adding a Display Name of the Server Address
  • Editing the Display Name of the Server Address
  • Deleting the Display Name and the IP Address of a Server
  • Importing a List of the Display Names and IP Addresses of Servers
  • Exporting the List of the Display Names and IP Addresses of Servers
  • Clearing the List of the Display Names and IP Addresses of Servers