earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server, WorkStation
Functionalities: User Management
12/3/2024

Building Operation WorkStation Window

Use the Building Operation WorkStation window to log on to WorkStation.

 
action_zoom_plus_stroke Building Operation WorkStation
Figure: Building Operation WorkStation

Table: Building Operation WorkStation

Component

Description

U ser name

Type the user name of your EcoStruxure Building Operation user account. For more information, see User Accounts and User Account Groups .

Password

Type the password of your EcoStruxure Building Operation user account or of your Windows user account.

Domain

Type the name of the EcoStruxure Building Operation domain that you want to log on to. If you do not enter a domain, you are logged on to the local domain. For more information, see Domains .

Server

Select the Server hypertext transfer protocol option for communication with the EcoStruxure BMS server.

Enter an EcoStruxure BMS server name or an IP address for the EcoStruxure BMS server you want to log on to.

Log on as

Click to log on to WorkStation with your Windows user account. For more information, see User Accounts and User Account Groups .

Remember me on this computer

Select to save the entered information. The information is automatically filled in the next time you log on.

Log on

Click to log on to WorkStation.

Click here to learn more about Building Operation

Click to open the WebHelp home page.

  • WorkStation Account Validation
  • Wrong Domain, User Name or Password
  • Domains
  • Server is not Available
  • Logon Button Greyed Out
  • User Accounts and User Account Groups
  • User Accounts and User Account Groups
  • Domains
  • Display Names and IP Addresses of Servers Drop-Down List Box