earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
10/30/2025

Property Context Menu – New Submenu

Use the New submenu to create new objects.

 
action_zoom_plus_stroke Property context menu - New submenu
Figure: Property context menu - New submenu

Table: Property Context Menu - New Submenu

Command

Description

Alarm

Click to open the Create Object wizard where you create an alarm. For more information, see Create Object Dialog – Naming the Object Page .

An alarm monitors a variable and alerts you if the monitored variable matches the configured alarm conditions. For more information, see Alarms Overview .

Trend

Click to open the Create Object wizard where you create trend logs, trend log lists, or trend charts. For more information, see Create Object Dialog – Naming the Object Page .

The function of a trend log is to log the variable that it is connected to and store the records. For more information, see Trends Overview .

  • Property Context Menu
  • Property Context Menu