earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
10/30/2025

Creating a Naming Convention

You create the naming convention to ease the naming in the create object process.

Show More
action_close

The naming convention eases the naming in the create object process. In order to ensure that a naming standard is followed on the site, you can choose a name from a list of suggestions in the create wizard. You can either compile your own list of names or use an existing naming standard such as SEBA Naming Convention which is developed by Schneider-Electric, ecoxpert.se.com/design/selector-tools/seba-naming-convention

The naming convention needs to contain a column with names of objects. You can also add columns with descriptions or information about semantic type.

You prepare the list of names in a CSV-file using UTF-8 encoding.

To create a naming convention
  1. Create a spreadsheet file with at least one columns, containing names for objects.

    Tip:

    You can add more columns, for instance "description" or "semantic type". In the process naming the object, the form in Create Object wizard will get filled in independently if you start typing the name or the description.

  2. You compile your own list of names or use an existing naming standard such as SEBA Naming Convention, which is developed by Schneider-Electric.

  3. Save the list on your Hard Drive in CSV file format using UTF-8 encoding.

  4. In WorkStation, in System Tree, select Engineering.

  5. In the Engineering tab, in Naming Convention , click Import

     
    action_zoom_plus_stroke

  6. In your Hard Drive, browse to your CSV file and click Open .

  • Naming Convention
  • Object Names
  • Engineering Properties – Engineering Tab
  • Create Object Dialog – Naming the Object Page