earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Semantic
12/3/2024

Edit Semantic Items

arrow1_rotationSemantic Labels arrow1_rotationSemantic Relations arrow1_rotationSemantic Paths arrow1_rotationSemantic Class arrow1_rotationUpdating the Semantic Model

You can edit the semantic items in a number of ways.

Semantic Labels

Semantic labels are labels that helps to identify a semantic item. Semantic labels can be edited or removed. Semantic labels can also be replaced using Find and repalce.

For more information, see Adding or Editing a Label of a Semantic Item .

For more information, see Find and Replace Labels and Paths on Semantic Items .

Semantic Relations

Semantic relations are relations between semantic items.

For more information, see Removing a Relation Between Semantic Items .

Semantic Paths

The semantic path defines the relation between a semantic item and an EBO object. Semantic path can be changed or removed. Semantic paths can also be replaced using Find and repalce.

For more information, see Editing the Semantic Path .

For more information, see Find and Replace Labels and Paths on Semantic Items .

Semantic Class

All semantic items are part of a class. You can change the class of a semantic item.

For more information, see Changing the Class of a Semantic Item .

Updating the Semantic Model

Update the semantic model if you have added alarms or trend logs to an EBO object that already have a relation to a semantic item. When you update the semantic model the alarm and trend log is added to the semantic model.

For more information, see Updating the Semantic Model .

  • Semantic Engineering Workflow
  • Opening the Semantic Engineering View
  • Adding or Editing a Label of a Semantic Item
  • Find and Replace Labels and Paths on Semantic Items
  • Removing a Relation Between Semantic Items
  • Editing the Semantic Path
  • Find and Replace Labels and Paths on Semantic Items
  • Changing the Class of a Semantic Item
  • Updating the Semantic Model