earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Semantic
12/3/2024

Changing the Class of a Semantic Item

You can change the class of a semantic item.

Show More
action_close

Semantic engineering is the process describing an EcoStruxure Building operation database using semantic s .

All engineering regarding semantics is done in WorkStation.

Semantic Engineering Workflow

Use this workflow to make a semantic description of your EcoStruxure Building Operation database.

For more information, see Semantic Engineering Workflow .

To change the class of a semantic item
  1. In the Semantic editing table , right-click the semantic item.

  2. Click Change class .

  3. In the class field, type the class you want to use.

  • Opening the Semantic Engineering View
  • Clearing the Semantic Editing Table View
  • Creating Semantic Objects using Drag and Drop
  • Adding a Semantic Item to the Semantic Model
  • Adding a Semantic Point to the Semantic Model
  • Copying and Pasting a Semantic Item
  • Editing the Semantic Path
  • Updating the Semantic Model