earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Semantic
12/3/2024

Clearing the Semantic Editing Table View

You clear the semantic editing table view to make it easier to get an overview.

Show More
action_close

Semantic engineering is the process describing an EcoStruxure Building operation database using semantic s .

All engineering regarding semantics is done in WorkStation.

Semantic Engineering Workflow

Use this workflow to make a semantic description of your EcoStruxure Building Operation database.

For more information, see Semantic Engineering Workflow .

To edit the Semantic editing table view
  • Right-click In the Semantic Editing Table .

    • To remove all semantic items from the view, right-click any where in the Semantic Editing Table view and click Clear view .

    • To remove a particular semantic item from the Semantic Editing Table view, right-click the semantic item and click Remove from view .

The removed semantic items are not deleted from the semantic model.

  • Opening the Semantic Engineering View
  • Creating Semantic Objects using Drag and Drop
  • Adding a Semantic Item to the Semantic Model
  • Adding a Semantic Point to the Semantic Model
  • Copying and Pasting a Semantic Item
  • Editing the Semantic Path
  • Changing the Class of a Semantic Item
  • Updating the Semantic Model