earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Basic Functionality
12/3/2024

Backup and Restore using WebStation

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded and uploaded from the server.

Scheduled backup must be done using WorkStation.

For more information, see Backup .

  • Backup and Restore Overview
  • Backing up and Restoring using WebStation
  • Backup