earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Basic Functionality
12/3/2024

Backup and Restore Overview

arrow1_rotationBackup arrow1_rotationRestore arrow1_rotationBACnet Backup and Restore arrow1_rotationExternal Log Storage Backup and Restore arrow1_rotationArchiving Overview arrow1_rotationComparison of Backup and Restore Methods arrow1_rotationRetain Level arrow1_rotationBackup and Restore using WebStation

You backup your EcoStruxure BMS server data so that it can be restored after damage or loss due to hardware or software failures, security threats, or application testing.

The EcoStruxure Building Operation software provides backup and restore capabilities that preserve both configuration and historical data on an as-needed or periodic basis.

Backup

Backup is the process of copying and storing data so that the copy can be used to restore data if a loss occurs. You can also use a backup to revert to an older version. In the EcoStruxure BMS, you can perform backups on an all EcoStruxure BMS servers and their devices. EcoStruxure BMS server backups should take place during non-business hours.

For more information, see Backup .

Restore

Restore is the process of restoring data to an original or former state. Using Restore, you can revert to a previous snapshot of the EcoStruxure BMS server data despite any configuration changes made since the last backup. In the EcoStruxure BMS, Restore is a manual process designed to avoid the accidental overwriting of current EcoStruxure BMS server data.

For more information, see Restore .

BACnet Backup and Restore

BACnet Backup uses a binary file format to back up an entire device. Specifically, BACnet Backups comprise the entire contents of the selected device, such as associated objects, properties, bindings, historical data, and related proprietary configuration data.

For more information, see BACnet Backup and Restore .

External Log Storage Backup and Restore

The External Log Storage feature uses an external database administered by a combination of TimescaleDB and PostgreSQL software. The EcoStruxure Building Operation backup and restore feature cannot be used to back up and restore the External Log Storage data. Instead you use the backup and restore function of TimescaleDB. See the TimescaleDB documentation for instructions.

For more information, see External Log Storage Backup and Restore .

Archiving Overview

Archiving is the process of preserving historical data, which is comprised of selected events and extended trend logs. For example, some facilities are required to maintain archives to comply with government regulations. Another example is in secure facilities where they must maintain records of who logged in or who changed setpoints. Archiving is not a backup function because archive data cannot be imported back into the system.

For more information, see Archiving Overview .

Comparison of Backup and Restore Methods

There are two Backup and Restore methods:

  • EcoStruxure Building Operation Backup and Restore

  • BACnet Backup and Restore

You can select the backup and restore method that suits your EcoStruxure BMS server data storage and retrieval requirements.

For more information, see Comparison of Backup and Restore Methods .

Retain Level

In the EcoStruxure BMS servers, variable values are primarily stored in flash memory in order to have their values survive power fail and server shutdown. However, values that are often collected are only stored in the SDRAM memory. This is done to protect the flash memory in the field server.

For more information, see Retain Level .

Backup and Restore using WebStation

A subset of backup and restore features are available in WebStation.

For more information, see Backup and Restore using WebStation .

  • Backup
  • Restore
  • BACnet Backup and Restore
  • External Log Storage Backup and Restore
  • Archiving Overview
  • Comparison of Backup and Restore Methods
  • Retain Level
  • Backup and Restore using WebStation