earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Semantic
12/2/2024

Tenant Repositories Dialog Box

Use the Tenant Repositories dialog box to add and edit tenant repository.

 
action_zoom_plus_stroke Tenant Repositories dialog box
Figure: Tenant Repositories dialog box

Table: Tenant Repositories Dialog Box

Component

Description

 
action_zoom_plus_stroke

Add

Click to add a tenant repository. For more information, see Tenant Repository .

 
action_zoom_plus_stroke

Edit

Click to edit a tenant repository. Click to add a tenant repository. For more information, see Tenant Repository .

 
action_zoom_plus_stroke

Remove

Click to remove a tenant repository from the list. For more information, see Tenant Repository .

Lead object

​Enter the object that acts as the lead for this object.

For more information, see Lead and Shadow Relationship .

  • Semantic Overview
  • Semantic Engineering Overview
  • Tenant Repository
  • General Information Properties – Basic Tab