earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Semantic
12/2/2024

Semantic Tenant Repository Workflow

Use this workflow to create and configure tenant repositories.

 
action_zoom_plus_stroke Semantic tenant repository workflow
Figure: Semantic tenant repository workflow
Set the semantic permissions

Make sure that you have semantic permission.

For more information, see Configuring Semantic Permissions .

Add and configure a tenant repository on the EcoStruxure Building Operation server

You add a tenant repository in EcoStruxure Building Operation to create a tenant repository on the EcoStruxure Building Operation server define the filter that you want to use on the semantic information and to create a password for the tenant repository.

For more information, see Adding a Tenant Repository on the EcoStruxure Building Operation Server .

Create tenant repositories on the semantic database

When you have added and configured the tenant repositories on the EcoStruxure Building Operation server you create the repositories on the semantic database. All tenant repositories on the EcoStruxure Building Operation server are created at the same time when you create the tenant repositories on the semantic database.

For more information, see Creating Tenant Repositories on the Semantic Database .

Populate the tenant repositories

When the semantic configuration is done you upload the semantic data matching the configured filter to the semantic database. Whenever you make any changes to the semantic model on the EcoStruxure Building Operation server you must populate the tenant repositories.

For more information, see Populating a Tenant Repository .

Connect a user group to the tenant repository

The last step is to connect the EcoStruxure Building Operation to a specific tenant repository.

For more information, see Connecting a User Group to the Tenant Repository .

  • Semantic Overview
  • Semantic Engineering Overview
  • Semantic Tenant Repository Workflow
  • Tenant Repository
  • Adding a Tenant Repository on the EcoStruxure Building Operation Server
  • Creating Tenant Repositories on the Semantic Database
  • Populating a Tenant Repository
  • Connecting a User Group to the Tenant Repository