earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Device Administrator, FDP Server
Functionalities: Engineering, License Management
3/6/2025

Returning Demo Licenses from Field Servers

You remove demo licenses after they have expired or when you commission a site.

You cannot activate or deactivate licenses when the field server is connected using a USB cable.

Show More
action_close

Use this workflow to return demo licenses from field servers.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Return demo licenses from field servers workflow
Figure: Return demo licenses from field servers workflow
Return demo licenses from field servers

Return the demo licenses from your automations servers using Device Administrator.

You must return all the demo licenses from the field servers before you remove the demo license from Device Administrator.

For more information, see Removing Demo Licenses File from Device Administrator .

For more information, see Returning All Demo Licenses from the Selected Field Servers .

Do not remove the demo licenses file from Device Administrator until all demo licenses are removed from your field servers.

Remove demo licenses file from Device Administrator

When you have returned all demo licenses from your field server you can remove the demo licenses file from Device Administrator if you are not going to use the demo license again.

For more information, see Removing Demo Licenses File from Device Administrator .

To return demo licenses from field servers
  1. In Device Administrator, click Servers .

  2. Select Show licenses .

  3. In the Assign Licenses view, in the License status column, click the Show products button

     
    action_zoom_plus_stroke
    .

  4. In the Assign column, in the row for Demo , clear Assign .

  5. In the Deactivate Demo License dialog box, click Yes .

  6. Click OK .

Repeat the procedure for all other field servers you want to return demo licenses from.

  • Demo Licensing Overview
  • Return Demo Licenses from Field Servers Workflow
  • Removing Demo Licenses File from Device Administrator
  • Assign Licenses View