earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Device Administrator, ​License Administrator, ​License Server
Functionalities: License Management
12/3/2024

Demo Licensing Overview

Demo licenses are used for demonstration purposes, training, or when building a site.

There are two types of demo licenses:

  • EcoStruxure Building Operation Software Demo Licenses on Windows. These licenses are managed by License Administrator and handles licenses on Enterprise Server and Enterprise Central.

  • Field server Demo Licenses. These licenses are managed by Device Administrator and handles licenses on field servers.

EcoStruxure Building Operation Software Demo License on Windows Management

Demo licenses for EcoStruxure Building Operation software are local, bound to the computer, and cannot be shared.

The license file used to activate demo licenses can only be used once per computer and is time-limited. The demo license is installed on License Server from a license file with the extension .asr. Demo licenses must be activated on the same computer that runs WorkStation, Enterprise Server or Enterprise Central.

For more information, see EcoStruxure Building Operation Software Demo Licenses on Windows Management .

Field Server Demo License Management

You add and return licenses on field servers using Device Administrator.

For more information, see Field Server Demo License Management .

  • Licensing Overview
  • Demo Licensing Overview
  • EcoStruxure Building Operation Software Licensing Overview
  • EcoStruxure Building Operation Software Demo Licenses on Windows Management
  • Field Server Demo License Management