earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Device Administrator, FDP Server
Functionalities: Security
12/2/2024

Temporarily Trusting an Invalid Certificate

You temporarily trust an invalid certificate when you are sure that you have a secure connection between Device Administrator and a field server.

Show More
action_close

You can check the status of certificates.

The certificate state is displayed, and can be changed, in the Certificate State column in Device Administrator.

Certificates can have tree states, invalid, invalid but temporarily trusted, and valid.

Invalid certificate

An invalid certificate is indicated by the icon

 
action_zoom_plus_stroke
.

When the certificate is invalid no communication between the Device Administrator and field server is allowed.

Invalid certificate temporarily trusted

An invalid certificate that is temporarily trusted is indicated by the icon

 
action_zoom_plus_stroke
.

When the invalid certificate is temporarily trusted communication between Device Administrator and the field server is allowed.

You can temporarily trust an invalid certificate to allow communication between Device Administrator and the field server.

For more information, see Temporarily Trusting an Invalid Certificate .

The trusting of the certificate is only valid for the current user session. If you close Device Administrator and re-open it the certificate is not trusted anymore.

Valid certificate

A valid certificate is indicated by the icon

 
action_zoom_plus_stroke
.

A valid certificate allow communication between Device Administrator and the field server. Valid certificates are the preferred state.

To temporary trust an invalid certificate
  1. In Device Administrator, click Servers .

  2. In the Certificate State row, click on the icon.

  3. In the Invalid Certificate dialog box, select Trust the certificate .

When you have completed the task that required that your trusted the invalid certificate, open the Invalid Certificate dialog box again and select Do not trust the certificate .

  • Certificate State
  • Certificates Managed using Device Administrator
  • Invalid Certificate Dialog Box