earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
6/2/2025

XLSX Report Trigger Settings Tab

Use the XLSX Report Trigger Settings tab to configure the trigger settings for the XLSX report.

 
action_zoom_plus_stroke XLSX Report Trigger Settings Tab
Figure: XLSX Report Trigger Settings Tab

Table: XLSX Report Trigger Settings Tab

Component

Description

Time period

Select the time period.

Trigger variable

Enter the variable that triggers the XLSX report.

Trigger condition

Select when you want the XLSX report to be triggered: when the trigger variable changes to true, changes to false, or all changes.

Alarm activation schedule

Add an alarm activation schedule to trigger the XLSX report.

Notify on transition to

Select the alarm states that trigger the notification.

 
action_zoom_plus_stroke

Add condition

Add a condition to trigger the XLSX report.

  • XLSX Reports Overview
  • XLSX Reports Workflow
  • XLSX Report Template Tab
  • XLSX Template Tab
  • Context Configuration – Template Tab
  • Context Configuration – Calculation Tab
  • Context Configuration – Misc Tab