earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
11/19/2025

Adding the Context to the XLSX Spreadsheet

You add the context to include the objects you want to display in the spreadsheet.

Show More
action_close

XLSX Report is a simplification of the Notification report function. Instead of creating trigger-notification objects and report template objects you create a XLSX Report object. The XLSX Template, which contains an XLSX document, is created for you and stored as a sub object of the XLSX report object.

To use the XLSX reports function you need to have MS Excel or similar installed on your computer.

The XLSX report feature support Custom Types.

The XLSX report is a WorkStation feature only.

The XLSX report object

The XLSX Reports object exposes all the report settings, including Trigger and Distribution.

The XLSX template

Defines how the XLSX report is displayed.

XLSX data bindings

XLSX reports data bindings are references to the objects that contains the data. You can have multiple contexts sharing the same data binding if you for example want to have different calculations of the same data.

XLSX reports data bindings are specified in the XLSX template object. The bindings are exposed in the XLSX report object as object paths. The path can be relative or absolute.

XLSX data context and substitution code

The XLSX data context describes the data type. The data context also specifies the properties and columns that are included in the report.

Each data context is represented by a context code, that is, a substitution code, for example <Consumption_Log/>. The substitution code must be copied and pasted into the spreadsheet. The substitution codes for each column are automatically generated by the XLSX report function when the XLSX report is generated or previewed.

To add the context to the XLSX spreadsheet
  1. In the XLSX Template dialog box, click Template context .

  2. In the Template context list, double-click the template context you want to include in the report.

  3. At the bottom of the Template context list, copy the substitution code text in the Copy to spreadsheet box.

  4. Click Edit with spreadsheet .

  5. Paste the substitution code text where you want it in the spreadsheet.

  6. Close and save the spreadsheet.

  • XLSX Reports Overview
  • XLSX Reports Workflow
  • Creating and Configuring the XLSX Template
  • Creating an XLSX Report
  • Creating and Configuring the XLSX Template
  • XLSX Report Template Tab
  • Context Configuration – Template Tab