earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Alarms
10/30/2025

Context Configuration – Template Tab

Use the Context Configuration – Template tab to configure the template.

 
action_zoom_plus_stroke Context Configuration – Template tab
Figure: Context Configuration – Template tab

Table: Context Configuration – Template Tab

Component

Description

Context name

Type a name for the context.

Binding data

Select, edit, or create binding data.

Include column header

Select to include column headers in the report.

Include unit

Select to include the unit you want to include in the report.

Use horizontal layout

Select if you want a horizontal layout.

Use default layout

Clear Use default layout if you want to manually select available properties.

Available properties

Displays available properties that can be included in the report.

Selected properties

Select available properties to be included in the report. Use default layout must be cleared for the properties to be selected.

Copy to spreadsheet

Displays the substitution code to be used in the spreadsheet. Copy the substitution code and paste it into the spreadsheet where you want to display it.

Preview with test data

Displays the data that you have configured.

  • XLSX Reports Overview
  • XLSX Reports Workflow
  • XLSX Report Template Tab
  • XLSX Template Tab
  • Context Configuration – Template Tab
  • Context Configuration – Calculation Tab
  • Context Configuration – Misc Tab