earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server
Functionalities: Security
12/2/2024

Importing a Certificate to Windows Certificate Store

You import certificates to Windows trusted storage to increase the security.

Show More
action_close

You can use Windows Certificate Store to store certificates used for Enterprise Server and Enterprise Central authentication. In this case you do not use WorkStation for the storage functions. Instead you use Certmgr.exe, Windows Certificate Manager Tool.

However, WorkStation is still used for activating the certificates you want to use.

Certificates with Elliptic Curve Cryptography (ECC cipher / encryption) are supported when authorizing servers in EcoStruxure Building Operation.

Use this workflow to import and activate certificates in Windows Certificate Store.

For more information, see Windows Certificate Store for Enterprise Server and Enterprise Central Workflow .

To import a certificate to Windows Certificate Store
  1. On the computer running Enterprise Server or Enterprise Central, open certlm.msc, Windows Certificate Manager Tool.

  2. Import the certificate in the Certificates folder in the Personal folder.

  3. Import the associated root certificate in the Certificates folder in the Trusted Root Certificate Authorities folder.

  4. Make sure that the private key for the certificate is marked as exportable.

  • Windows Certificate Store for Enterprise Server and Enterprise Central Workflow
  • Windows Certificate Store for Enterprise Server and Enterprise Central
  • Certificates Tab
  • Importing a Certificate to Windows Certificate Store
  • Activating a Certificate from Windows Certificate Store Using WorkStation