earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Basic Functionality
12/3/2025

Editing a Text File Using WebStation

You can edit a text file to keep it updated.

Show More
action_close

You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.

You can edit the documents and then save them again using WorkStation. You cannot edit and save documents using WebStation.

Important:

When you log off or are automatically logged off, any unsaved changes in the document are not saved in the database. Make sure that you save changes in open documents frequently.

To edit a text file using WebStation
  1. In WebStation, in the System Tree pane or List view, click the text file you want to edit.

  2. Edit a .txt file by writing in the text area. Click Save .

You can only edit the text file you have access to.

  • Basic Functions
  • How Documents Work
  • Opening a Document