earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation, WebStation
Functionalities: Basic Functionality, Graphics
12/12/2025

Enabling a Loop Device or a Zone from a Graphic

You enable a loop device or a zone to make them operate in the fire detection system.

Warning Warning

COMPROMISED FUNCTIONALITY

Ensure that no obstructions preventing normal operation are present before you enable loop devices or zones.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Important:

Ensure that there is no smoke, dust, or any other condition, near the loop device or in the zone, that can affect the fire detection and result in a false alarm.

To enable a loop device or a zone from a graphic
  1. In WorkStation or WebStation, in a fire graphic, click a disabled loop device or zone. On the Actions menu, click the multiselect icon

     
    action_zoom_plus_stroke
    to select several loop devices. Use the selector
     
    action_zoom_plus_stroke
    to browse existing selections and click one of them.

  2. On the Actions menu, click the Enable option.

  3. Click the Apply button

     
    action_zoom_plus_stroke
    to enable the objects.

  4. Click  Yes  to execute the action, click  No  to cancel it.

If you have enabled loop devices, those with no remaining disablements are enabled and their updated state is displayed in the graphic. If you have enabled zones, they are enabled and their updated state is displayed in the graphic.

  • Fire Graphic Menus