Executing System Commands from a Fire Graphic
You execute system commands to reset, silence, or re-sound alarms or alerts, for example when testing the fire detection system.
Warning
|
|
REDUCED RESPONSE TO FIRE
Ensure that there is no need for evacuation before you reset or silence alarms or pre-alarms.
Comply with any applicable legislation, regulations, standards, and guidelines regarding actions to be taken before you reset or silence alarms or pre-alarms.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
|
Important:
Executing a system command on a type of alarms or alerts affects all alarms or alerts of that type in the entire fire detection system, not only those displayed in the graphic.
To execute system commands from a fire graphic
In WorkStation or WebStation, in a fire graphic, in the
Actions
menu, click the system command button
action_zoom_plus_stroke
.
To execute reset commands, click the
Reset
button
action_zoom_plus_stroke
and then select the command you want to execute.
To execute silence commands, click the
Silence
button
action_zoom_plus_stroke
and then select the command you want to execute.
To execute re-sound commands, click the
Re-sound
button
action_zoom_plus_stroke
and then select the command you want to execute.
Click the
Apply
button
action_zoom_plus_stroke
to execute the command.
Fire Graphic Menus