earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Alarms
12/3/2024

Assignment Properties

Use the Assignment properties to configure which user or user group receives the assignment request.

 
action_zoom_plus_stroke Assignment properties
Figure: Assignment properties

Table: Assignment Properties

Component

Description

Status

Select Disabled to deactivate the assignment function.

​Schedule

Enter the schedule or other multistate variable that contains the value that is to be used to activate the assignment.

Active value

Enter the value, generated by the connected schedule or other multistate variable, that is to activate this assignment object.

Assigned to

Click the browse button to open the Users and Groups dialog box where you select the EcoStruxure Building Operation user or user group to receive the assignment request. For more information, see Users and Groups Dialog Box .

  • Alarm Control Panel Objects in Multiple Servers
  • User Cannot Be Assigned to an Alarm
  • General Information Properties – Basic Tab
  • Users and Groups Dialog Box