earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Alarms
12/3/2024

Cause Notes

A cause note specifies the problem that caused the alarm. Cause notes are grouped by category, with possible alarm causes listed in each group. When an alarm is triggered, you can easily report the causes that triggered the alarm by selecting the predefined choices.

 
action_zoom_plus_stroke Cause Notes dialog box
Figure: Cause Notes dialog box

Reporting the cause of the alarm is either voluntary or mandatory. You can configure the alarm so the user is required to report the causes when certain events occur, such as when an alarm is disabled.

​Cause notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics.

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Cause Notes View
  • Configuring Forced User Actions
  • Adding a Cause Note to an Alarm
  • Adding a Cause Note to an Alarm in WebStation
  • Editing a Cause Note
  • Editing a Cause Note using WebStation
  • Creating a Cause Note
  • Creating a Cause Note using WebStation
  • Import and Export of Supporting Objects