You use graphics to display building overviews, display the status of detectors and alarms, display the value of sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.
A graphic that contain links to documents, such as Microsoft Word or Adobe PDF, can be opened in WorkStation and WebStation. The associated programs, in this case Microsoft Word or Adobe Reader, has to be installed on the computer running WorkStation or WebStation.
action_zoom_plus_stroke
Figure:
A Graphic with links and interactive components like gauges in WorkStation
Fire Graphic Headers
If a default graphic is defined in the fire detection system configuration, the
Home
button
action_zoom_plus_stroke
in the fire graphic header displays the default graphic.
If a navigation menu is created in the fire detection system configuration, the
Navigation
button
action_zoom_plus_stroke
in the fire graphic header displays the navigation menu.
Fire Graphic Menus
The graphic menus in EcoStruxure Fire Operation are used to display alarms and alerts in a graphic. The menus are also used to apply commands on either loop devices and zones in a graphic or on the fire detection system.
For more information, see Fire Graphic Menus
.
Sets of Icons in Fire Graphics
There are two sets of icons in fire graphics, default icons and Swedish icons.
For more information, see Sets of Icons in Fire Graphics
.