earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: ​License Administrator, ​License Server
Functionalities: License Management
12/3/2024

Configuring the License Server Recovery Settings  

You configure License Server recovery settings to ensure that the License Server restarts if it unexpectedly stops. 

Show More
action_close

License Server manages licenses administered by License Administrator.

An EcoStruxure BMS that uses Licenses Administered by License Administrator must contain at least one License Server.

License Server is a Microsoft Windows service named Building Operation License Server.

Configure the License Server to automatically restart if it unexpectedly stops. For more information, see Configuring the License Server Recovery Settings   .

You can access License Server through a web interface. For more information, see Accessing License Server Using the Interface .

With a default installation, the License Server port range is set to 27000-27009. A valid number is any unused port between 0 and 64000.

If the License Server uses other ports than the default port range 27000-27009, the port has to be added in front of the @ in the License Server address on the WorkStation, Enterprise Server, or Client tools.

To configure the license server recovery settings
  1. On the computer running License Server, open the Services management console.

    Note:

    In Windows, open the Run dialog box and type services.msc .

  2. Right-click Building Operation License Server .

  3. Select Properties .

  4. Click the Recovery tab.

  5. In the First failure box, select Restart the Service .

  6. In the Second failure box, select Restart the Service .

  7. In the Subsequent failures box, select Restart the Service .

  8. Click OK .

  • License Server