earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, FDP Server
Functionalities: Basic Functionality
12/3/2024

Control Panel – Backup and Archiving

Use the Backup and Archiving options on the Control Panel to create new backup rules, diagnose backup or restore issues, and view the current status of an EcoStruxure BMS server.

 
action_zoom_plus_stroke Control Panel – Backup and archiving
Figure: Control Panel – Backup and archiving

Table: Control Panel – Backup and Archiving

Component

Description

Backup Rules

Click to open the Backup Rules view where you manage backup rules. You can also modify the backup schedule associated with the backup rule. For more information, see Backup Rules View .

Backup Sets

Click to open the Backup Sets view where you manage backup sets. For more information, see Backup Sets View .

Backup and Restore Manager

Click to open the Backup and Restore Manager where you view current backup and restore statuses and configure Purge settings for an Enterprise Server. For more information, see Backup and Restore Manager on the Enterprise Server .

Archiving

Click to open the Archive Settings where you enable the archiving function, set delay, and select the format of the archive file. For more information, see Archiving Settings Properties – Basic Tab .

  • Backup and Restore Overview
  • Backup Rules View
  • Backup Sets View
  • Backup and Restore Manager on the Enterprise Server
  • Archiving Settings Properties – Basic Tab