earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: ​License Administrator, ​License Server
Functionalities: Basic Functionality
12/2/2024

Installing the License Administrator and the License Server

You install License Administrator and License Server to ​administer the activation, return, repair, check out, and the check in of the EcoStruxure Building Operation licenses. An EcoStruxure BMS has to include one software license server. The License Administrator has to be installed on all clients or servers that run any licensed products.

Show More
action_close

Depending on your needs, you can install all EcoStruxure Building Operation products or a few products, such a single field server with a connected WorkStation.

WorkStation

​WorkStation is the interface where you supervise your EcoStruxure BMS. In WorkStation you can also create, modify, and delete some of the objects that are used to build an EcoStruxure BMS.

Important:

​​Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation.

When you install WorkStation, you have the option to install the bundled tools: Graphics Editor, Script Editor, Menta Editor, Function Block Editor, and WorkPlace Tech. WorkStation is required to run these client tools.

For more information, see WorkStation .

Graphics Editor

​You can use Graphics Editor to create and edit graphics representing a site and the devices that make up the site.

Important:

​​You have to have a valid Graphics Editor license to start the ​Graphics Editor.

The installation of Graphics Editor is bundled into the WorkStation installation package.

For more information, see Graphics Editor .

Script Editor

Script Editor is a text programming tool you use to create Script programs that control and monitor building automation systems. For example, in WorkStation, you can create a basic program, called OfficeLights, to control lighting and ventilation in a room based on occupancy.

Important:

Ensure that you have a working and available Script license. A working license is required to start Script.

The installation of Script Editor is bundled into the WorkStation installation package.

For more information, see Script Editor Program Creation .

Menta Editor

Menta Editor is a graphical programming tool for Xenta 208/300/401 LonWorks device, which you use to create function block programs that control and monitor building automation systems. For example, you create a program to control an air handling unit.

Important:

Ensure that you have a working and available Menta Editor license. A working license is required to start the Menta Editor software.

The installation of Menta Editor is bundled into the WorkStation installation package.

For more information, see TAC Menta ., Technical Manual (04-00030).

Function Block Editor

Function Block Editor is a graphical programming tool for EcoStruxure BMS servers and MP controllers, which you use to create function block programs that control and monitor building automation systems. For example, you create a basic program, called OfficeLight, to control lighting in a room based on occupancy.

Important:

​Ensure that you have a working and available Function Block Editor license. A working license is required to start the Function Block Editor software.

The installation of Function Block Editor is bundled into the WorkStation installation package.

For more information, see Function Block Editor Overview .

WorkPlace Tech

The WorkPlace Tech component of WorkStation consists of two graphical tools: WorkPlace Tech Monitor and WorkPlace Tech Editor. With WorkPlace Tech Editor, you can create, modify, monitor, and troubleshoot MNL LonWorks and MNB BACnet device applications. With WorkPlace Tech Monitor, you can monitor and troubleshoot applications in MNL LonWorks and MNB BACnet devices.

Important:

Ensure that you have a working and available WorkPlace Tech license. A working license is required to start the WorkPlace Tech Editor or WorkPlace Tech Monitor software.

The installation of WorkPlace Tech is bundled into the WorkStation installation package, and is specific to the particular version of WorkStation in that package.

Important:

The WorkPlace Tech Editor component requires the installation of the appropriate version of Microsoft Visio.

For more information, see Information Technology System Planning Guide .

Enterprise Central

Enterprise Central is the hierarchical EcoStruxure BMS server at the top of the system architecture hierarchy of a large Building Management System. Enterprise Central is primarily used for administration and data aggregation in an EcoStruxure BMS that has multiple Enterprise Servers. From one location, you can manage operations across large Building Management Systems that have multiple Enterprise Server subsystems.

For more information, see Enterprise Central .

Enterprise Server

Enterprise Server is the hierarchical EcoStruxure BMS server at the top of the system architecture hierarchy of a medium size Building Management System, or at the middle of the hierarchy in a large system. Enterprise Server is primary used for administration, system supervision and engineering of field servers. Enterprise Server aggregates data that can be accessed by Enterprise Central.

Important:

​Ensure that you have a working and available Enterprise Server license. A working license is required to start the Enterprise Server.

For more information, see Enterprise Server .

Software Administrator

​The Software Administrator installs with the Enterprise Server installation package. You use the Software Administrator to start and stop the Enterprise Server service and configure the ports of the Enterprise Server.

For more information, see Software Administrator .

Device Administrator

The Device Administrator is used to configure and upgrade the software of EcoStruxure BMS servers through a network or USB connection.

License Administrator

The License Administrator administers the activation, return, and repair of licenses.

For more information, see License Administrator .

License Server

The License Server manages the administration of network licenses. An EcoStruxure BMS running with network licenses must contain at least one License Server.

For more information, see License Server .

The License Server Installation is bundled into the License Administration installation package.

Language Package

​At the main installation, WorkStation contains English and languages that are avaílable at the time. To support a language, WorkStation needs the specific language package.

For more information, see Language Packages .

To install the License Administrator and License Server
  1. Double-click on the License Administrator installation file to start the installation wizard.

  2. Click Yes to confirm that you want to run the License Administrator installation package.

  3. Click Next .

  4. In the License Agreement page, make sure that you agree with the End User License Agreement (EULA) and then click I Agree .

  5. In the Installation Folder page, browse to the folder where you want to install License Administrator and License Server and then click Next .

    Important:
    • When upgrading to a later version, the installation path is changed to the default installation folder for that version. The default installation folder is always located on the C: drive

    • The complete installation path can have maximum 115 characters.

    Note:
    • EcoStruxure Building Operation products are installed in the same folder that you selected for the first product you installed

  6. In the Choose Components page, select the components you want to install and then click Next .

  7. In the License Server Configuration page, in the License Server Address box, type @ and then type the address to the license server.

    Note:
    • If the License Server uses a port other than the default port range 27000-27009, type the port number in front of @. For example, 567@localhost.

    • Use a semicolon to separate addresses to different License Servers.

  8. Click Install .

  9. In the Installation Complete page, click Next .

    Note:

    Click Show details to follow the progress of the installation.

  10. Click Finish .

It is recommended that you configure the license server recovery settings to ensure that the license server restarts if it unexpectedly stops. For more information, see Configuring the License Server Recovery Settings   .

  • Installation Overview
  • Installation Wizard – Choose Components Page
  • Installation Wizard – License Server Configuration Page
  • Installation Example
  • Products
  • Configuring the License Server Recovery Settings