earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WorkStation
Functionalities: Basic Functionality
12/2/2024

Menu Bar

Use the Menu bar to access the different file menus in WorkStation.

 
action_zoom_plus_stroke Menu bar
Figure: Menu bar

Table: Menu Bar

Component

Decription

File

Click to open the File menu, where you log off from the system, import and export information, print, and create new objects. For more information, see File Menu .

Edit

Click to open the Edit menu, where you edit objects in the system. For more information, see Edit Menu .

View

Click to open the View menu, where you display or hide Workspace components. For more information, see View Menu .

Actions

Click to open the Actions menu, where you carry out commands for objects selected in the System Tree pane or List View. For more information, see Actions Menu .

Window

Click to open the Window menu, where you close or navigate between open windows. For more information, see Window Menu .

Tools

Click to open the Tools menu, where you open the Control Panel and the Options dialog box. For more information, see Tools Menu .

Help

Click to open the Help menu, where you access the help and view information about the WorkStation version number. For more information, see Help Menu .

  • File Menu
  • Edit Menu
  • View Menu
  • Actions Menu
  • Window Menu
  • Tools Menu
  • Help Menu