earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Alarms
12/3/2024

Create Multistate Alarm Wizard – Alarm Trigger Page

Use the Alarm Trigger page to configure the trigger settings of the multistate alarm.

 
action_zoom_plus_stroke Multistate alarm trigger page
Figure: Multistate alarm trigger page

Table: Multistate Alarm Trigger Page

Component

Description

 
action_zoom_plus_stroke

Add row

Click to add another alarm condition that triggers the alarm.

 
action_zoom_plus_stroke

Remove row

Click to remove an alarm condition.

between

Select a range. If the monitored variable is within this range, the alarm is triggered.

equal to

Select a value. If the monitored variable is equal to this value, the alarm is triggered.

Monitored variable

​Enter the path to the variable that is monitored by the alarm.

Disable alarm

​Displays the present state of the alarm. For more information, see Alarm States .

Alarm delay

​Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered.

Reset delay

​Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset.

Shunt variable 1

​Enter the shunt variable that is used to enable or disable the alarm. For more information, see Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. For more information, see Shunt Variables .

Operator

Select AND or OR to add logic between the first and the second shunt variable. For more information, see Shunt Variables .

Shunt variable 2

​Enter the second shunt variable that is used to enable or disable the alarm. For more information, see Shunt Variables .

Invert

Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. For more information, see Shunt Variables .

 
action_zoom_plus_stroke

Set u nit

​Enter the unit of the alarm.

  • Multistate Alarms
  • Create Alarm Wizard – Presentation Page
  • Create Alarm Wizard – User Action Page
  • Create Alarm Wizard – Attachment Page
  • Create Object Dialog – Naming the Object Page