Use the Alarm Trigger page to configure the trigger settings of the out of range alarm.
|
Component |
Description |
|
Upper limit |
Enter the highest value the monitored variable can increase to before the alarm is triggered. |
|
Lower limit |
Enter the lowest value the monitored variable can decrease to before the alarm is triggered. |
|
Deadband |
Enter the range the monitored variable has to pass within the normal range before the alarm is reset. |
|
Monitored variable |
Enter the path to the variable that is monitored by the alarm. |
|
Disable alarm |
Select to disable the alarm, for example, before deployment. |
|
Alarm delay |
Enter the time, in seconds, the alarm has to be within the alarm criteria before the alarm is triggered. |
|
Reset delay |
Enter the time, in seconds, the alarm has to be within the reset criteria before the alarm state is changed from alarm to reset. |
|
Shunt variable 1 |
Enter the shunt variable that is used to enable or disable the alarm. For more information, see Shunt Variables . |
|
Invert |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. For more information, see Shunt Variables . |
|
Operator |
Select AND or OR to add logic between the first and the second shunt variable. For more information, see Shunt Variables . |
|
Shunt variable 2 |
Enter the second shunt variable that is used to enable or disable the alarm. For more information, see Shunt Variables . |
|
Invert |
Select to invert the shunt value, that is, enable the alarm when the shunt value is active and disable the alarm when the shunt value is inactive. For more information, see Shunt Variables . |
|
Set u nit Enter the unit of the alarm. |