earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: User Management
12/2/2024

Pane Properties

Use the Pane properties to configure the settings of the pane.

 
action_zoom_plus_stroke Pane properties
Figure: Pane properties

Table: Pane Properties

Component

Description

Show toolbar

Select Yes to show the toolbars for the pane component.

Default dock position

Select where to place the pane in the workspace.

Default visibility

Select Hidden to hide the pane.

Dipslay name

Type the pane name that is to be displayed. Display name is available only in Workstation.

Initial path

Enter the path to the pane component.

  • Workspace Management
  • General Information Properties – Basic Tab