earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Central, Enterprise Server, Esmi Sense FDP
Functionalities: Basic Functionality
12/2/2024

Simple Math Operator Properties - Basic Tab

Configure the Simple Math Operator properties Basic tab to add, subtract, multiply, or divide one value from another when you perform tests.

 
action_zoom_plus_stroke Simple math operator
Figure: Simple math operator

Component

Description

Operator

Select the operator, add, subtract, multiply, or divide.

In1

Input value 1.

In2

Input value 2.

Value

Displays the calculated value.

  • Creating a Utility Object
  • General Information Properties – Basic Tab
  • References Tab
  • Signal Generator Properties - Basic Tab
  • Create Object Dialog – Naming the Object Page
  • Forced Values