earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: ​License Administrator, ​License Server
Functionalities: License Management
10/30/2025

Starting License Administrator

You start License Administrator to administer the licenses on the License Server and define the address to the License Servers for licenses that are not administered using Centralized Licensing.

Show More
action_close

The License Administrator administers the activation, return, and repair of licenses.

You use License Administrator to activate EcoStruxure Building Operation software licenses on the License Server. For more information, see License Administrator .

During the installation of WorkStations or Enterprise Servers, you can change the network address to the License Server where licenses are available for check out. The address to the License Server can later be entered or edited through License Administrator on the computer that hosts the licensed product.

When you use the default setting during installation, you do not have to change the network address. For more information, see EcoStruxure Building Operation Software Licensing Installation and Location .

The address to a License Server must begin with @ and is either a hostname or IP address. If the communication to the License Server is through a port other than the default port range 27000-27009, the port number is defined in front of the @, Port-number@hostname.

Table: Examples of License Server Address

Address

Description

19650@localhost

Connects to localhost through port 19650

@server2c.schneider-electric.com

Connects to License Server server2c.schneider-electric.com through a port in the default port range 27000-27009

14650@192.166.248.2

Connects to License Server 192.166.248.2 through port 14650

To separate License Server addresses in License Administrator, use a semicolon.

To start License Administrator
  1. Click Start , point to All Programs, and then click Schneider Electric EcoStruxure .

  2. Click Building Operation x.x .

  3. Click Building Operation License Administrator .

  4. Click Yes to confirm that you want to run License Administrator .

  • License Administrator
  • Activating Licenses Using License Administrator