earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: ​License Administrator, ​License Server
Functionalities: License Management
10/30/2025

Activating Licenses Using License Administrator

You activate EcoStruxure Building Operation software licenses, from the License Activation Server, to make EcoStruxure Building Operation software licenses available.

Note:
  • This procedure requires that an entitlement with the licenses has been received. For more information, see Order Information Request .

    For more information on how to place an order, contact your EcoStruxure Building Operation vendor.

Show More
action_close

Use this workflow to add licenses administrated by License Administrator.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Licensing workflow
Figure: Licensing workflow
Licenses Administrated by License Administrator Installation and Location

Read the setup guide for installation and location of License Server and License Administrator.

For more information, see EcoStruxure Building Operation Software Licensing Installation and Location .

Install License Administrator and License Server

Install Licenses Administrator and License Server.

For more information, see Installing the License Administrator and the License Server .

Start License Administrator

Start License Administrator.

For more information, see Starting License Administrator .

Activate Licenses on License Administrator

Activate EcoStruxure Building Operation Software Licenses.

For more information, see Activating Licenses Using License Administrator .

Configure License Server Recovery Settings

Configure License Server to restart if it unexpectedly stops.

For more information, see Configuring the License Server Recovery Settings   .

To activate licenses using License Administrator
  1. In License Administrator, click the Licenses tab.

  2. On the Licenses toolbar, click the Add license from entitlement ID button

     
    action_zoom_plus_stroke
    .

  3. In the Add License dialog box, in the Enter license entitlement ID box, type the entitlement ID that contains the licenses to activate. The entitlement ID is printed on the entitlement.

  4. Click OK .

  5. In the Licenses View, in the Activate column, select the number of license to activate.

  6. Click Activate .

  7. Click Close .

  8. Click Restart now to restart the License Server and activate the license.

The activated licenses are now available on the License Server.

  • EcoStruxure Building Operation Software Licensing Installation and Location
  • Licenses Administrated by License Administrator Workflow